csm_Leuze_GettyImages-900256746_edited_RGB_1400px_66fa51bd2f

Technologieën

Nieuwe technologieën en de digitalisering van de industrie veranderen niet alleen waardecreatieprocessen, maar openen ook nieuwe bedrijfsmodellen en perspectieven. Wij richten ons voortdurend op de technologische uitdagingen en thema's in onze klantenmarkten. Dit is de voorwaarde voor onze hoogwaardige productontwikkeling en consultingexpertise.

AI: Sensorgegevens als basis voor efficiënte processen

startseiten_slider_desktop_sw

Kunstmatige intelligentie kan worden gebruikt om productieprocessen nog intelligenter, flexibeler en zuiniger te maken met behulp van gegevens die door veldcomponenten worden gegenereerd. AI-algoritmen analyseren grote hoeveelheden gegevens en bepalen kengetallen of noodzakelijke acties om de productiviteit van de fabriek continu te verbeteren.

 

Lees meer 

Technology report: Clear view guaranteed with vision sensors

17 dec 2024 | Technologieën
Simple_Vision_IVS-1048-DCR-1048_700x500px
Three aspects of sensor technology are particularly important in image processing for industrial automation: performance, flexibility and usability. Simple Vision sensors meet these requirements. They are as easy to operate as optical sensors, plus they are as powerful as camera systems. The Sensor People from Leuze offer this concept as a quick and straightforward introduction to vision technology.

Technology report: AutoID-Technology - quo vadis?

9 sep 2024 | Technologieën
APIC_IL_PA_BCL300i_line_scanner_through_roll_wl_500x700px
Automatic identification systems such as 1D/2D-code and RFID readers are tried-and-tested, indispensable technologies for controlling industrial production processes and logistics workflows in the supply chain. At the same time, Industry 4.0 and IIoT have put digitization at the focus of advancing automation. What demands will in future be placed on modern identification systems? Has the classic reader, which forwards a code via a serial interface to a control, become obsolete?

Technology report: RFID or bar code?

10 okt 2022 | Technologieën
PPIC_Bar_code_readers_500x700px_V2
Two identification technologies – RFID and bar code – are competing for the favor of users: With the promise of making a decisive contribution to realizing an automated transparent production and supply chain to meet the requirements of Industry 4.0. But which technology is the right one today? Has the bar code outlived its purpose? This article takes stock of the current situation with respect to modern identification technologies and casts a critical eye over each of them.