csm_Leuze_GettyImages-900256746_edited_RGB_1400px_66fa51bd2f

기술

새로운 기술과 산업의 디지털화로 인해 가치 창출 방법이 변화하고 있을 뿐만 아니라 새로운 비즈니스 모델과 관점이 열리고 있습니다. 저희는 고객의 시장에서 기술적 도전과 중요한 주제를 지속적으로 해결하고 있습니다. 이는 고성능 제품 개발 및 컨설팅 기술을 위한 전제 조건입니다.

AI: 효율적인 공정을 위한 기반으로서의 센서 데이터

startseiten_slider_desktop_sw

필드 구성 요소에서 생성된 데이터는 인공지능을 통해 생산 공정을 더욱 스마트하고 유연하며 경제적으로 만듭니다. AI 알고리즘을 이용할 경우 대량의 데이터를 평가하고 주요 수치 또는 필요한 조치를 결정하여 플랜트 생산성을 지속해서 개선할 수 있습니다.

 

자세히 알아보기 

Technology report: Clear view guaranteed with vision sensors

2024. 12. 17. | 기술
Simple_Vision_IVS-1048-DCR-1048_700x500px
Three aspects of sensor technology are particularly important in image processing for industrial automation: performance, flexibility and usability. Simple Vision sensors meet these requirements. They are as easy to operate as optical sensors, plus they are as powerful as camera systems. The Sensor People from Leuze offer this concept as a quick and straightforward introduction to vision technology.

Technology report: AutoID-Technology - quo vadis?

2024. 9. 9. | 기술
APIC_IL_PA_BCL300i_line_scanner_through_roll_wl_500x700px
Automatic identification systems such as 1D/2D-code and RFID readers are tried-and-tested, indispensable technologies for controlling industrial production processes and logistics workflows in the supply chain. At the same time, Industry 4.0 and IIoT have put digitization at the focus of advancing automation. What demands will in future be placed on modern identification systems? Has the classic reader, which forwards a code via a serial interface to a control, become obsolete?

Technology report: RFID or bar code?

2022. 10. 10. | 기술
PPIC_Bar_code_readers_500x700px_V2
Two identification technologies – RFID and bar code – are competing for the favor of users: With the promise of making a decisive contribution to realizing an automated transparent production and supply chain to meet the requirements of Industry 4.0. But which technology is the right one today? Has the bar code outlived its purpose? This article takes stock of the current situation with respect to modern identification technologies and casts a critical eye over each of them.