Technology report
Gapless safety
In applications where corridor supply vehicles interact at transfer stations with a direct connection to a danger zone, operation must be as safe and efficient as possible: Throughout the entire area, the safety system must be able to differentiate reliably between forklift trucks and, in some cases, also people. This is possible using a Leuze safety solution for multi-station access guarding in forklift truck logistics.
Person or vehicle?

Conventional muting with a high residual risk
An obvious approach uses a type of "muting" with induction loops as a trigger signal. The induction loops, which are embedded in the floor before every transfer station as "muting sensors", make it possible, in principle, to differentiate between high-lift trucks and people. However, to differentiate SAFELY, additional evaluation measures are generally required. Nevertheless, the main dealbreaker for this approach is ultimately the muting requirements specified by standards such as IEC 62046, which are not met. This is because, if all transfer stations are safeguarded jointly by an active opto-electronic protective device (AOPD) used for muting, the presence of a forklift truck on one loop pair triggers the muting function for the entire area – i.e. across all stations. At that moment, people can enter the danger zone along with the forklift truck, undetected and without realizing. While the high-lift truck stands on the induction loop, the muting function is active and the safety function of the AOPD is overridden. At the same time, the lateral distances between the muting object (here, the forklift truck) and the fixed limit are far too great and therefore no longer compliant. As a result, a conventional muting approach is not suitable for this type of application. In addition to the large amount of effort required to install the induction loops, the approach has residual risks and does not comply with the muting requirements of standards.
Better suited intelligent safety concepts

Interruption-free operation

An optimal combination: Laser, ultrasound and radar
The Sensor People from Leuze offer this concept as a safety solution in a complete package. A core component is the RSL 400 safety laser scanners. They are installed vertically above the transfer stations so that they can safeguard the entire access area. A practical feature of the RSL 400 is that it can safeguard multiple transfer stations simultaneously due to its operating range of up to 8.25 meters and the parallel operation of various protective fields. This reduces the installation effort and helps to create a cost-optimized system design. The Leuze project teams flexibly adjust the protective field configurations that are appropriate for the respective system to the conditions on site. The safety laser scanners are characterized by their robust operation. They filter out objects such as dust and particles due to their high angular resolution of 0.1 degrees – this makes the sampling rate 3x higher than that of conventional scanners. Other components of the safety solution include ultrasonic and radar sensors that are used for each station. A Siemens safety control, together with the associated Leuze safety program, is used to control the overall system.
Danger averted
For system operators, this approach to multi-station access guarding pays off: It is suitable for retrofitting existing systems as well as for new systems. The solution reliably differentiates between forklift trucks and operators, and operation is not interrupted. Even protection against bypassing is optimized and tampering prevented. The safety concept meets the requirements for performance level d according to EN ISO 13849-1 and therefore contributes significantly to reducing the risks at transfer stations. The safety integrity level according to EN IEC 62061 is SIL 2. In addition, the solution can easily be scaled to the number of stations at any time – this offers flexibility for later extensions. The Leuze safety experts are happy to advise anyone interested in this concept at any time. They provide support relating to the safety solution from the target/actual analysis to the hardware selection including accessories, to the configuration, start-up support and validation of the application.

The author
![]() |
Matthias Bristle Product Manager Safety Solutions Leuze electronic GmbH + Co. KG Phone: +49 7021 573-0 Email: matthias.bristle@leuze.com Web: www.leuze.com |